i.mx6SL or i.mx6SX ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6SL or i.mx6SX ?

866 Views
lee_ee
Contributor II

Dear all

Between i.mx6SL and i.mx6SX,which processor's power consumption is lower to use for mobile handheld device with battery power supply.

Thanks

0 Kudos
Reply
1 Reply

707 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The i.MX6SL has a single-core ARM Cortex-A9, while the i.MXSX has one Cortex-A9 core and one Cortex-M4 core. Depending of your application, the additional M4 core could be useful or a consumer.

You could refer to “Electrical Characteristics” section of the proper Datasheet, and to application note AN4580 “i.MX 6SoloLite Power Consumption Measurement” in order to get an idea of which kind of test cases could be applied for the i.MX6 SoloX.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply