i.mx6 solo平台移植Android4.4版本,出现init: untracked pid 2343 exited等异常

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6 solo平台移植Android4.4版本,出现init: untracked pid 2343 exited等异常

3,925件の閲覧回数
yongheluo_hotma
Contributor III

您好,
我在公司的设备上移植Android4.4版本时,出现
init: untracked pid 2343 exited
及:
GraphicBufferAlloc::createGraphicBuffer(w=1024, h=600) failed (Out of memory), handle=0x0
错误,

系统无法正常运行,界面无显示。

我的硬件平台是:i.mx6 Solo, 1G DDR3, 2G nand.

我的问题是:
1)针对上述错误,是否有相关的解决思路?
2)i.mx6 solo 能否支持Android版本?如果支持的话,选择哪个Android版本会比较好?是否有推荐的下载资源链接?(在移植Android4.4版本之前,我也有尝试将Android7.1.2 移植到我们的设备上,也是跑在init进程,就卡在某个service上了。)
3)敝司这个设备(i.mx6 Solo, 1G DDR3, 2G nand)是否满足Android版本的最低要求?

Log详见附件。


谢谢!
罗永和

ラベル(4)
0 件の賞賛
10 返答(返信)

3,487件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

关于你上述问题回复如下:

1、你这里硬件2G的Nand跑Android系统的话太小了。

2、只要是官网发行的支持i.mx6solo的Android的版本都是支持的。

3、如果你这里Android的系统都是写到2G的Nand的话是有问题的,2G太小了装不下。Android系统flash最好是参考我们官网开发板的设计,8G的。 Linux系统的话4G可以满足,4G装Android都小。

希望如上回复对您有帮助。
Have a great day,
TIC Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

3,487件の閲覧回数
yongheluo_hotma
Contributor III

Dear Rita,

     感谢您的回复。

     目前,我们量产的设备上,用的Linux版本,用的1G的Nand flash(因为是行业应用,Nand Flash比较小)。我们希望推出Android版本,以适应客户的需要。

     对于Android4.4版本,我编译出来的sytem.img目前只有380M左右,按我理解,从分区来看,应该是够的,所以就没有往此处想。(android 7.1 我编译出来的版本是700多MB,理论上也是够的)。

     针对空间不足的问题,我现在想切换到SD卡的启动模式试试看。

     请帮忙提供一下贵司官网发行的Android 4.4的下载链接(因为我们的板子是针对贵司的SabreSD设计的),我重新移植一便;(之前的Android 4.4版本是迅为开发板上的,虽然我全部移植过来了,但还是担心有些差别)

    

       谢谢!

    Yonghe.Luo

0 件の賞賛

3,487件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

你可以换SD卡试一下。关于Android4.4.3源码链接:

https://www.nxp.com/webapp/sps/download/preDownload.jsp 

https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true 

Tool

i.MX 6 Series Manufacturing Toolkit for Android KK4.4.3 Release
Have a great day,
TIC Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

3,487件の閲覧回数
yongheluo_hotma
Contributor III

Dear Rita,

    上述的几个链接,均出现“Page Not Found”,请再帮忙确认一下。

     

     我准备换SD卡试试,或者换个4G的EMMC。

  

      谢谢!

    Yonghe.Luo

Page Not Found

The page you requested cannot be found.

Possible reasons for missing pages, and what you can do:

  • If you typed a URL in the Address bar, make sure the URL was spelled correctly.
  • If you used a bookmark, please delete it and navigate from the homepage.
  • If you cannot find a product or page and need technical assistance, please enter a service request.
  • This page may not be available in the language you selected
0 件の賞賛

3,487件の閲覧回数
yongheluo_hotma
Contributor III

Dear Rita,

   更正一下:其中,mfg tools可以下。

  谢谢!

Yonghe.Luo

0 件の賞賛

3,487件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

请问源码现在可以下载么?不可以的话,我云盘分享给你。

还有你说用SD卡或者emmc试的话,4G的大小Linux系统是没有问题的,android还是建议使用8G的。

0 件の賞賛

3,487件の閲覧回数
yongheluo_hotma
Contributor III

Dear Rita,

    源码还是不能下,请帮忙用云盘分享给我。我会用8G的SD卡先试试。

    非常感谢!

    Yonghe.Luo

0 件の賞賛

3,487件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Yonghe Luo,

链接: https://pan.baidu.com/s/1jJfW6rG 密码: duji

Have a nice day
Rita

0 件の賞賛

3,487件の閲覧回数
yongheluo_hotma
Contributor III

Dear Rita,

      看了一下,资料里面是“KK4.4.3_2.0.1 is a patch release for the KK4.4.3_2.0.0 release.”,没有包含KK4.4.3_2.0.0相关资料。

      不过,我现在已经从贵司官网上下载到KK4.4.3_2.0.0相关的资料,并下载了源码,由于时间关系,目前没有移植完成。

      感谢您的支持!谢谢!

    Yonghe.Luo

      

0 件の賞賛

3,487件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Yonghe Luo,

不客气的~~

Have a nice day

Rita

0 件の賞賛