MY-i.MX6-CB200 core board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MY-i.MX6-CB200 core board

1,255 Views
cherryzheng
Contributor II

MY-IMX6-CB200 Core Board

  •      CPU:MX6QP/Q/U/S: Compatible with the

automotive, industrial, consumer level

  •      Memory: DDR3 1GB, up to 2GB
  •      Storage: SPI NorFlash/4GB EMMC,

Up to 64 GB EMMC

  •      Power supply: 5V
  •      Size: 40mm x 68mm
  •      Working Temperature:

Consumer(-20°C..85°C), up to 1.2 GHz

Automotive(-40°C..105°C), AEC-Q100, up to 1 GHz

Industrial (-40°C..85°C), up to 800 MHz

 

Main Features:

  •      4x ARM Cortex-A9 up to 1GHz per core at work
  •      200 Mtri/s 1000Mpxl/s, OpenGL ES 2.0&Halti, CL EP
  •      1MB L2cache
  •      GPU 2D(Vector Graphics)
  •       32KB instruction and data cache
  •       Vivante GC355 300Mpxl/s, Open VG1.1
  •      NEON SIMDmedia accelerator
  •      GPU 2D(Composition)
  •      GPU 3D
  •      Vivante GC320 600Mpxl/s, BLIT
  •      Vivante GC2000
  •      Video Decode:1080p 60h.264
  •      Hardware BCH(up to 20 corrections)
  •      Video Encode:1080p30H. 264BP 2x720p encode
  •      Camera Interface
  •      Types: 1x 20-bit parallel, MIPI-CSI-2(2 lanes), three simultaneous inputs

 

OS Support:

  •      Linux 3.0.35/Linux 3.14.52/Linux-4.1.15, Android4.4.2/Android5.1, QT4.8.5/QT5, Ubuntu12.04/Ubuntu16.04

hardware configuration

core board main model

CPU

memory capacity

storage capacity

boot mode

burning mode

other

MY-IMX6-CB200

i.MX 6QP

1G / 2G

eMMC: 4G ~ 64G

SPI Flash

two bit dialing

standard configuration:memory 1G,storage 4G

 

i.MX 6Q

1G / 2G

eMMC: 4G ~ 64G

SPI Flash

two bit dialing

standard configuration:memory 1G,storage 4G

 

i.MX 6U

1G

eMMC: 4G ~ 64G

SPI Flash

two bit dialing

standard configuration:memory 1G,storage 4G

 

i.MX 6S

512M / 1G

eMMC: 4G ~ 64G

SPI Flash

two bit dialing

standard configuration:memory 512M,storage 4G

CB200-6Q7C.jpg

If you would like to know more about our products, please visit our website www.myzr.com.cn or email to enquiry@myzr.com.cn.

 

Labels (1)
0 Kudos
0 Replies