i.mx6 pwm-backlight

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx6 pwm-backlight

跳至解决方案
8,443 次查看
lawrencehuang
Contributor I

how can i add pwm-backlight in my kernel? i use RIoTboard and linux L3.10.17_1.0.0 but can't find where can add it.

thanks!

标签 (1)
0 项奖励
回复
1 解答
3,411 次查看
csotoalonso
Contributor III

Ooops! Totally forgot about it.

If you want to change the PWM device, you don't have to change any source code, just the DTS file for your board. Pretty much as I did for my board:

  1. In the backlight section, change <&pwm4 0 5000000>;to pwm3
  2. Enable pwm3:  you need to modify the phandle for pwm3 and change the status to "okay"
  3. In pincontrol, add a group for your pwm and set the correct PAD assignments for your output pin (SD1_DATA1, I presume)

And that's all. As Artur Petukhov pointed out, you'll have your backlight control exported to sysfs, so you can change its brightness value.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,411 次查看
art
NXP Employee
NXP Employee

Please refer to the Section 6.2.2 of the document attached.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,411 次查看
csotoalonso
Contributor III

Hi,

you need to do a couple of things:

  1. Add pwm-backlight support in your kernel, as a built-in module or as a loadable module.
  2. Modify your DTB to add backlight support for your board. As a reference, you could take a look to the imx6qdl-sabresd.dtsi file.

Also, you can see what I did to my board here https://community.freescale.com/thread/337988  It's for a iMX25 board, but the DTB configuration is similar.

0 项奖励
回复
3,411 次查看
lawrencehuang
Contributor I

Hi Carlos:

thanks for your reply. but i have some point not understand.

1. in imx6solo_RIoTboard.dts have pwm-backlight

        backlight {

        compatible = "pwm-backlight";

        pwms = <&pwm4 0 5000000>;

        brightness-levels = <0 4 8 16 32 64 128 255>;

        default-brightness-level = <7>;

2. if modify to use pwm3 (SD1_DATA1) where can modify it. because i can't fine the file in source code. could you give me the fiel path or which way to modify it?

0 项奖励
回复
3,412 次查看
csotoalonso
Contributor III

Ooops! Totally forgot about it.

If you want to change the PWM device, you don't have to change any source code, just the DTS file for your board. Pretty much as I did for my board:

  1. In the backlight section, change <&pwm4 0 5000000>;to pwm3
  2. Enable pwm3:  you need to modify the phandle for pwm3 and change the status to "okay"
  3. In pincontrol, add a group for your pwm and set the correct PAD assignments for your output pin (SD1_DATA1, I presume)

And that's all. As Artur Petukhov pointed out, you'll have your backlight control exported to sysfs, so you can change its brightness value.

0 项奖励
回复