i.mx28evk no eth0 with power from USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx28evk no eth0 with power from USB

Jump to solution
1,308 Views
chris321
Contributor IV

Hello Community,

if I run the i.mx28evk(L2.6.35) with power from the 5V jack all things work fine. I use udhcpc to get an IP.

But if i power it from the USB port J82 (with S3:ON and S16:USB 5V) the Ethernet won't work.

I don't get dhcp responses with power from USB.

$ ifconfig eth0

eth0      Link encap:Ethernet  HWaddr 00:01:9F:02:4D:72

          BROADCAST MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

          Base address:0x8000

$ udhcpc

udhcpc (v1.15.0) started

eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1)

Sending discover...

Sending discover...

Sending discover...

...

I think it's the same problem like in this thread eth0 problem in imx28 evk but I'm not sure. Are there any solutions for this?


Chris


Labels (2)
0 Kudos
Reply
1 Solution
1,051 Views
FranciscoCarril
Contributor V

Did you already applied the FEC patches that are available in our web page?

i.MX285 Product Summary Page

View solution in original post

0 Kudos
Reply
2 Replies
1,051 Views
chris321
Contributor IV

I'm not sure, I've put the two patches in the folder ltib/rpm/BUILD/linux/patches and renamed them to match the consecutive numbers of the other 571 patches.

then I've rebuild the kernel with ./ltib -f kernel

0 Kudos
Reply
1,052 Views
FranciscoCarril
Contributor V

Did you already applied the FEC patches that are available in our web page?

i.MX285 Product Summary Page

0 Kudos
Reply