Hi,
We are using QNX on i.mx6 sabrelite board for my application , it is working fine.
But now we want WiFi on SDIO and Bluetooth on UART, so we selected WL18XXSDIO board.
Now we are using SDIO interface and
WiFi enable , WiFi irq, TX, RX CTS, RTS , BTenable pins from camera connector.
Now we want to mux these camera pins into WiFi enable, BT enable, WiFi irq, RX, TX, CTS, RTS.
We made below changes in the below file
bsp-freescale-mx6q-sabrelite-SDP6.6/src/hardware/startup/boards/imx6x/sabrelite/mx6q_gpio.c
Could you please suggest , Is these changes are enough to work or we need to make any otherchanges
please guide us
Thank you for your support
Hi sandesh
please look on boundary devices wifi implementation examples:
Differences between the Sabre Lite and Nitrogen6X i.MX6 development boards
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------