iMX6UL - Connect unused ADDR lines on DDR3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL - Connect unused ADDR lines on DDR3?

1,123 Views
ehwsma
Contributor I

Hi,

I'm currently working on the design of a board which uses a i.MX6UL + DDR3 RAM memory.

At the moment we selected a 1Gb DDR3 (x16), but we might change it to 2Gb in the future.

The only difference when switching between capacity is the number of address lines used:

- Only ADDR[0..12] for 1Gb

- ADDR[0..13] for 2Gb

- ADDR[0..14] for 4Gb

...

As unused ADDR lines are recommended to be NC, is it an issue if those lines are connected after all to ensure higher capacity compatibility?

Thanks

Sébastien

Labels (1)
Tags (2)
0 Kudos
Reply
5 Replies

880 Views
ehwsma
Contributor I

Hi Igor,

I mean, is it ok to mount a 1Gb DDR3 (with only ADDR[0..12] required) when the board was initially designed for a 4Gb DDR3 (with ADDR[0..14] routed between CPU and DDR component) ?

In that case, CPU ADDR[13;14] would be routed to NC pads of DDR3.

Thanks

Best regards,

Sébastien

0 Kudos
Reply

880 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sébastien

 

yes CPU ADDR[13;14] be routed to NC pads of DDR3

will be fine.

 

Best regards
igor

0 Kudos
Reply

880 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sébastien

yes i.MX6UL address lines can be left unconnected if not used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

880 Views
ehwsma
Contributor I

Hi Igor,

Thanks for your reply.

Actually my suggestion was the opposite: Can I left it CONNECTED while not used? So that I'm higher capacity proof.

Thanks

0 Kudos
Reply

880 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sébastien

 

could you clarify "CONNECTED while not used" ?

 

Best regards
igor

0 Kudos
Reply