Hello,
we observe sometimes a problem that our device hangs after a reboot, if the U-Boot 2017.03 starts the kernel 4.1.41.
In this case we only see "Starting kernel ..." at the serial console and our display becomes white with grey stripes.
With different waiting times, we can locate the issue to the four functional calls in the function ipu_disable_channel (drivers/mxc/ipu3/ipu_common.c):
reg = ipu_idmac_read(ipu, IDMAC_CHA_EN(in_dma));
ipu_idmac_write(ipu, reg & ~idma_mask(in_dma), IDMAC_CHA_EN(in_dma));
ipu_cm_write(ipu, idma_mask(in_dma), IPU_CHA_CUR_BUF(ipu->devtype, in_dma));
ipu_cm_write(ipu, tri_cur_buf_mask(in_dma), IPU_CHA_TRIPLE_CUR_BUF(ipu->devtype, in_dma));
The function ipu_disable_channel disables the IPU channels, which ist already activated by the u-boot the show our splash screen.
Unfortunately, it is very difficult to narrow down the issue further.
Has anybody an idea, how we analyze the problem further?
Kind regards
Mark
Solved! Go to Solution.
Hi Igor,
thanks for the links. We have reviewed the patches and fixed the IPU driver (ipu_common.c function ipu_init_channel) by bypassing the funcation calls:
_ipu_dp_init
_ipu_dc_init
Kind regards
Mark
Hi Mark
unfortunately "kernel 4.1.41" is not officially supported by nxp, sorry.
May be recommended to try official nxp linux, for example uboot imx_v2017.03 & L4.9.11_1.0.0 kernel
from nxp source.codeaurora.org/external/imx/ repository :
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.11_1.0.0_ga
https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=imx_v2017.03_4.9.11_1.0.0_ga
Documentation
Issues with non-nxp linux releases may be posted on meta-fsl-arm mailing list:
https://lists.yoctoproject.org/g/meta-freescale
Difference between offical nxp linux and other linux releases is described on
>Has anybody an idea, how we analyze the problem further?
as a general suggestion for crash one can try to run ddr test and update image with new calibration coefficients
found from ddr test
Best regards
igor
Hi Igor,
thanks for your feedback.
We have already tested the kernel 4.9.81 and this kernel crashes, too.
During the bring-up we have verified the DDR RAM Timing with the stress tool.
Kind regards
Mark
>The function ipu_disable_channel disables the IPU channels, which ist already
>activated by the u-boot the show our splash screen.
for uboot splash screen one can consider below nxp patches and port it :
Best regards
igor
Hi Igor,
thanks for the links. We have reviewed the patches and fixed the IPU driver (ipu_common.c function ipu_init_channel) by bypassing the funcation calls:
_ipu_dp_init
_ipu_dc_init
Kind regards
Mark