i.Mx 6ULL : serial download procedure using UART 1/2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx 6ULL : serial download procedure using UART 1/2

944 Views
HarshilSoni434
Contributor I

Hello There ,

For one of our project based on I.mx 6ULL

Actually we want to flash the nand using "serial download mode" through "UART 1/2" as mentioned in document "i.MX 6ULL Applications Processor Reference Manual".

But we are not able to do it based on procedure.

so Can you provide any procedure as well as tool(if require) for the same ?

Thanks and regards

0 Kudos
Reply
4 Replies

851 Views
HarshilSoni434
Contributor I

Hello @Sanket_Parekh  and NXP team,

Gentle Reminder ,

Request you to please provide update for the query we asked in previous reply .

 

Thanks and regards

0 Kudos
Reply

825 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

HI @HarshilSoni434 

I hope you are doing well
 
My apology for the delayed response.
 
Q)can UUU utility works with UART 1/2 ports if yes then is there any specific procedure ?
=>UUU supports the USB serial download mode but does not support operations through the UART.
 
If you would like more information about the same kidly refer to the threads below.
 
Thanks & Regards

Sanket Parekh

0 Kudos
Reply

919 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
I hope you are doing well
 
One can flash the NAND using UUU. Please look at the below script for the same.
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply

904 Views
HarshilSoni434
Contributor I

Hello @Sanket_Parekh and NXP team,

Thank you for the quick response ,

Actually we have tried using UUU with OTG port and UART1/2 port in Serial download mode,

but it works only with OTG port , we can able to successfully flash the NAND/EMMC through OTG using UUU but not through UART 1/2 ports.

 

when we try with UART 1/2 port  it's getting stuck in below logs :

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.39-0-gdcc404f

Wait for Known USB Device Appear...

 

So, that is why we asked here for any specific procedure for flashing using UART 1/2 ports,

can UUU utility works with UART 1/2 ports if yes then is there any specific procedure ?

 

Thanks and regards

 

0 Kudos
Reply