IMX6ULL - uuu via UART ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL - uuu via UART ?

1,023 Views
christian_oster
Contributor I

Hi, i would like to use uuu on a board with the imx6ull. I have no access to the usb, but to uart1 via a ftdi usb->232ttl adapter.

 

How to use uuu via COM-Port ? Processor is in Serial download mode via BOOT_MODE pins.

Labels (1)
0 Kudos
3 Replies

1,017 Views
igorpadykov
NXP Employee
NXP Employee

Hi christian_oster

 

unfortunately uuu does not support operation through uart, one

can try usb_loader:

https://github.com/boundarydevices/imx_usb_loader

https://freescale.jiveon.com/docs/DOC-95604

 

Best regards
igor

0 Kudos

1,011 Views
christian_oster
Contributor I

Can you please provide me windows bianries of imx_uart ?

0 Kudos

1,005 Views
igorpadykov
NXP Employee
NXP Employee

link below, Step 1. - Get and compile the "imx_usb_loader", shows how to compile it:

https://community.nxp.com/t5/i-MX-Processors/Guide-to-flash-iMX6-from-Linux/m-p/642187

 

Best regards
igor

0 Kudos