i.MX93 bootloader in LF_v6.1.36-2.1.0 not working?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX93 bootloader in LF_v6.1.36-2.1.0 not working?

跳至解决方案
784 次查看
hmk
Contributor II

Hi, I had a bluetooth issue on i.MX93 EVK...

However, the EVK shipped with a rather old BSP, so before going further with BT, I wanted to try the latest Linux 6.1.36_2.1.0 binaries. This includes imx-boot-imx93evk-sd.bin-flash_singleboot, which I believe I should be able to boot using:

uuu SDPS: boot -f imx-boot-imx93evk-sd.bin-flash_singleboot

However, the end result is that the board's USB interface disconnects and reconnects and there is no output whatsoever coming from the debug serial ports.  It does not boot.  uuu -lsusb tells me the board is still in SDPS mode.

Next I tried to dd imx-image-multimedia-imx93evk.wic onto an SD card and boot that.  Same end result: no output on debug ports, board does not boot.

To make sure uuu is actually working, I booted the original image from eMMC and dd'd /dev/mmcblk0boot0 to a file, and passed that to uuu:

uuu SDPS: boot -f mmcblk0boot0

End result: the original bootloader runs and we get in fastboot mode:

U-Boot SPL 2022.04-lf_v2022.04+gbb6108298d (Sep 05 2022 - 09:51:39 +0000)
SOC: 0xa0009300
LC: 0x40010
M33 prepare ok
Normal Boot
Trying to boot from BOOTROM
Boot Stage: USB boot
Find img info 0x&88000000, size 416
Download 1489920, Total size 1490944
NOTICE: BL31: v2.6(release):android-12.1.0_1.0.0-rc1-15-g9202efc9a
NOTICE: BL31: Built : 09:52:38, Sep 5 2022

U-Boot 2022.04-lf_v2022.04+gbb6108298d (Sep 05 2022 - 09:51:39 +0000)

CPU: i.MX93 rev1.0 at 1692 MHz
Model: NXP i.MX93 11X11 EVK board
DRAM: 2 GiB
...
Detect USB boot. Will enter fastboot mode!

So I know the board works and uuu works and the debug ports are fine.  But the bootloader in the latest BSP binary image does not boot.  What am I doing wrong?

0 项奖励
回复
1 解答
767 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @hmk!


Thank you for contacting NXP Support!

What silicon version do you have on your EVK?

The first version of the silicon is not compatible with the new Linux releases.

Sorry for the mistake!

Best Regards!
Chavira

在原帖中查看解决方案

2 回复数
756 次查看
hmk
Contributor II

Thanks Chavira.

The chip I have should indeed be the first version.  I've just downgraded to 6.1.22, which seems to work fine.

0 项奖励
回复
768 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @hmk!


Thank you for contacting NXP Support!

What silicon version do you have on your EVK?

The first version of the silicon is not compatible with the new Linux releases.

Sorry for the mistake!

Best Regards!
Chavira