i.MX8QM MX8-DSI-OLED1A color peoblem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8QM MX8-DSI-OLED1A color peoblem

866件の閲覧回数
YKL
Contributor I

The hardware I used is i.MX8qm(MX8-DSI-OLED1A) and the download is the official android_13.0.0_1.2.0 demo image.

The displayed image is not in the right color and cannot be touched.

Attach my image, please help me, thank you!

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

845件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what status for these two pictures? I mean how you get these pictures? just booting up?

0 件の賞賛
返信

842件の閲覧回数
YKL
Contributor I

The Android13 image demo was burned using the uuu tool (uuu: -d-mipi-panel) and output to MX8-DSI-OLED1A through mipi-dsi

After launch use the phone to shoot OLED1A display Android interface

0 件の賞賛
返信

817件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the quick start guide:

https://www.nxp.com.cn/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf

To test the MIPI panel display, connect the i.MX MIPI panel to the "MIPI DSI" port. OLED1 (RM67191) MIPI panel is supported, while OLED1A (RM67199) is not supported

0 件の賞賛
返信