Hi!
Trying to put the same pin configuration from imx8mp-evk.dts to out ".mex" using Config Tool for i.MX v10, there is no way to put the following values:
https://github.com/brgl/linux/blob/master/arch/arm64/boot/dts/freescale/imx8mp-evk.dts
&iomuxc { | |
pinctrl_fec: fecgrp { | |
fsl,pins = < | |
MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x3 | |
MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO 0x3 | |
MX8MP_IOMUXC_SAI1_RXD4__ENET1_RGMII_RD0 0x91 | |
MX8MP_IOMUXC_SAI1_RXD5__ENET1_RGMII_RD1 0x91 | |
MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2 0x91 | |
MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3 0x91 | |
MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC 0x91 | |
MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x91 | |
MX8MP_IOMUXC_SAI1_TXD0__ENET1_RGMII_TD0 0x1f | |
MX8MP_IOMUXC_SAI1_TXD1__ENET1_RGMII_TD1 0x1f | |
MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2 0x1f | |
MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3 0x1f | |
MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x1f | |
MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC 0x1f | |
MX8MP_IOMUXC_SAI1_RXD0__GPIO4_IO02 0x19 | |
>; | |
}; |
How can we put these values in the Config Tool v10?
The most approximate that we can put...
init_enet_pins: init_enet_pinsgrp {
fsl,pins = <
MX8MP_IOMUXC_ENET_MDC__ENET_QOS_MDC 0x00000006
MX8MP_IOMUXC_ENET_MDIO__ENET_QOS_MDIO 0x00000006
MX8MP_IOMUXC_ENET_RD0__ENET_QOS_RGMII_RD0 0x00000012
MX8MP_IOMUXC_ENET_RD1__ENET_QOS_RGMII_RD1 0x00000012
MX8MP_IOMUXC_ENET_RD2__ENET_QOS_RGMII_RD2 0x00000012
MX8MP_IOMUXC_ENET_RD3__ENET_QOS_RGMII_RD3 0x00000012
MX8MP_IOMUXC_ENET_RXC__CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK 0x00000012
MX8MP_IOMUXC_ENET_RX_CTL__ENET_QOS_RGMII_RX_CTL 0x40000012
MX8MP_IOMUXC_ENET_TD0__ENET_QOS_RGMII_TD0 0x00000016
MX8MP_IOMUXC_ENET_TD1__ENET_QOS_RGMII_TD1 0x00000016
MX8MP_IOMUXC_ENET_TD2__ENET_QOS_RGMII_TD2 0x00000016
MX8MP_IOMUXC_ENET_TD3__ENET_QOS_RGMII_TD3 0x00000016
MX8MP_IOMUXC_ENET_TXC__CCM_ENET_QOS_CLOCK_GENERATE_TX_CLK 0x00000016
MX8MP_IOMUXC_ENET_TX_CTL__ENET_QOS_RGMII_TX_CTL 0x00000016
>;
};
Thanks in advanced.
已解决! 转到解答。
@Charlie_Owz
Hello,
I do not think that it is possible to import Linux device tree
configuration to the i.MX Config Tool automatically. Moreover
export of the .mex file to Linux also is mainly manual procedure.
According to i.MX Config Tools User Manual, tool generated board-oriented
device tree (DTS) DTSI file is only a snippet, which contains basic device
tree elements, initial skeleton.
Content itself may be manually merged together with existing Linux BSP
device tree file(s) in order to apply the tool generated pins configuration.
For Your issue it is needed to define (manually) what pins are really
involved in Linux configuration and their settings, and then (manually)
configure them in the i.MX Config Tool.
From the document below:
properties:
fsl,pins:
description:
each entry consists of 6 integers and represents the mux and config
setting for one pin. The first 5 integers <mux_reg conf_reg input_reg
mux_val input_val> are specified using a PIN_FUNC_ID macro, which can
be found in <arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h>. The last
integer CONFIG is the pad setting value like pull-up on this pin. Please
refer to i.MX8M Plus Reference Manual for detailed CONFIG settings.
https://github.com/brgl/linux/blob/master/Documentation/devicetree/bindings/pinctrl/fsl%2Cimx8mp-pin...
For example, the line
MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x3
means, that SW_MUX_CTL_PAD_SAI1_RXD2 SW MUX Control Register (IOMUXC_SW_MUX_CTL_PAD_SAI1_RXD2)
( address 0x3033_0158) is used; bit field MUX_MODE = 4 ALT4 mux port: ENET1_MDC
From .h file
#define MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x158 0x3B8 0x000 0x4 0x0
https://github.com/brgl/linux/blob/master/arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h
Regards,
Yuri.
@Charlie_Owz
Hello,
I do not think that it is possible to import Linux device tree
configuration to the i.MX Config Tool automatically. Moreover
export of the .mex file to Linux also is mainly manual procedure.
According to i.MX Config Tools User Manual, tool generated board-oriented
device tree (DTS) DTSI file is only a snippet, which contains basic device
tree elements, initial skeleton.
Content itself may be manually merged together with existing Linux BSP
device tree file(s) in order to apply the tool generated pins configuration.
For Your issue it is needed to define (manually) what pins are really
involved in Linux configuration and their settings, and then (manually)
configure them in the i.MX Config Tool.
From the document below:
properties:
fsl,pins:
description:
each entry consists of 6 integers and represents the mux and config
setting for one pin. The first 5 integers <mux_reg conf_reg input_reg
mux_val input_val> are specified using a PIN_FUNC_ID macro, which can
be found in <arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h>. The last
integer CONFIG is the pad setting value like pull-up on this pin. Please
refer to i.MX8M Plus Reference Manual for detailed CONFIG settings.
https://github.com/brgl/linux/blob/master/Documentation/devicetree/bindings/pinctrl/fsl%2Cimx8mp-pin...
For example, the line
MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x3
means, that SW_MUX_CTL_PAD_SAI1_RXD2 SW MUX Control Register (IOMUXC_SW_MUX_CTL_PAD_SAI1_RXD2)
( address 0x3033_0158) is used; bit field MUX_MODE = 4 ALT4 mux port: ENET1_MDC
From .h file
#define MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x158 0x3B8 0x000 0x4 0x0
https://github.com/brgl/linux/blob/master/arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h
Regards,
Yuri.