i.MX8MM H.264 Features

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM H.264 Features

2,114 Views
vincentz63
Contributor IV

IMX8MMRM-i.MX 8M Mini Applications Processor Reference Manual, Rev. 1, 03/2019, page 4778 onwards describes the features of the VPU_H1 encoder that is available on the iMX8MMini.

Running "gst-inspect-1.0  vpuenc_h264" yields a very limited set of controllable properties.

From what I can see, only the bitrate, GOP and Q factors can be adjusted (see listing below).

How are we meant to make use of the other features of the encoder (setting the profile, CBR vs VBR, etc.) Do you expect us to edit the drivers (imx-hantro.so) and GStreamer vpuenc_h264 plugin ourselves? Looking at the doc, I doubt we have enough information to do that... Or am I missing something?

From what I can see others have asked similar questions but I don't think there has been a clear answer given so far:

i.MX8MM h.264 main profile support 

i.MX8M Mini VPU: Changing H.264 Profile 

Rank                     primary + 1 (257)
Long-name                IMX VPU-based AVC/H264 video encoder
...
Element Properties:
  name                : The name of the object
                        flags: readable, writable
                        String. Default: "vpuenc_h264-0"
  parent              : The parent of the object
                        flags: readable, writable
                        Object of type "GstObject"
  qos                 : Handle Quality-of-Service events from downstream
                        flags: readable, writable
                        Boolean. Default: false
  bitrate             : set bit rate in kbps (0 for automatic)
                        flags: readable, writable
                        Unsigned Integer. Range: 0 - 2147483647 Default: 0
  gop-size            : How many frames a group-of-picture shall contain
                        flags: readable, writable
                        Unsigned Integer. Range: 0 - 32767 Default: 30
  quant               : set quant value: H.264(0-51) (-1 for automatic)
                        flags: readable, writable
                        Integer. Range: -1 - 51 Default: -1

0 Kudos
Reply
1 Reply

1,708 Views
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the imx8MM reference manual, for profile, you can refer to the VPU H1 Register 18 (SWREG18), for the bitrate, 0 for automatic, which means VBR, for CBR, refer to the RM, Minimum: 10kbps,Maximum: 40 Mbps at 1080p 60 fps

0 Kudos
Reply