i.MX8MM ECSPI maximum transfer size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MM ECSPI maximum transfer size

ソリューションへジャンプ
1,213件の閲覧回数
sreedhar_appala
Contributor IV

Hi,

I am working with i.MX8MM EVK and 4.19-warrior yocto distribution.

We have interfaced a slave through ECSPI2 pins of i.MX8MM EVK.

From the Reference Manual, the FIFO size of Tx and Rx are 64 words each.

Could you please let me know.

What is the maximum SPI transfer size possible without DMA in ECSPI2 of iMX8MM?

What is the maximum SPI transfer size possible with DMA in ECSPI2 of iMX8MM?

Do you have any test code for validating the transfer size?

Thank you, Sreedhar

ラベル(3)
0 件の賞賛
返信
1 解決策
1,207件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sreedhar_appala

 

unfortunately I am not aware of test codes for validating the transfer size, for

burst size one can look at driver sources:

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-imx.c?h=imx_4.19.35_1.1.0

also may be useful:

https://community.nxp.com/t5/i-MX-Processors/imx8-ecspi-Master-Mode-with-SS-CTL-Control/m-p/984674

 

Best regards
igor

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,208件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sreedhar_appala

 

unfortunately I am not aware of test codes for validating the transfer size, for

burst size one can look at driver sources:

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-imx.c?h=imx_4.19.35_1.1.0

also may be useful:

https://community.nxp.com/t5/i-MX-Processors/imx8-ecspi-Master-Mode-with-SS-CTL-Control/m-p/984674

 

Best regards
igor

 

0 件の賞賛
返信
1,198件の閲覧回数
sreedhar_appala
Contributor IV

Hi igor,

Thank you, I have gone through the spi-imx.c and reference manual ecspix_conreg.

I understand the maximum SPI burst can be 4096 bits = 2^12 = 512 bytes. Same was coded in the spi-imx.c file.

Thank you once again.

Regards, Sreedhar

0 件の賞賛
返信