i.MX8M Mini support mipi-csi raw12 issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8M Mini support mipi-csi raw12 issue

2,052 次查看
tcchoub
Contributor I

Dear Sir,

Our sensor is [AR0135] + [1280 x 960] + [2 mipi lane with 800 Mpbs each lane]

Cureently, we meet the following issues when we want to capture mipi-csi aw12 on i.MX8M Mini.

(A). Reference from NXP community:

[i.MX8M Mini] => imx8m mini mipi csi采图异常  => No success to capture raw10

[i.MX8M] => Confirmed support for RAW12 through 4-lane CSI-2 sensor on i.MX8M?  => Success to Capture raw12


(B). The case which we capture video image with "multiple sensor images"(分屏)

#modify "fsl-imx8mm-evk.dts"
data-lanes = <2>;
csis-hs-settle = <17>;
csis-clk-settle = <0>;

#modify "mxc_mipi_csi.c"
{
.code = MEDIA_BUS_FMT_SBGGR12_1X12,
.fmt_reg = MIPI_CSIS_ISPCFG_FMT_RAW12,
.data_alignment = 16,
},

#modify "mx6s_capture.c"
{
.name = "RAWRGB12 (SBGGR12)",
.fourcc = V4L2_PIX_FMT_SBGGR12,
.pixelformat = V4L2_PIX_FMT_SBGGR12,
.mbus_code = MEDIA_BUS_FMT_SBGGR12_1X12,
.bpp = 2,
},

...................................................

...................................................

case V4L2_PIX_FMT_YUV32:
case V4L2_PIX_FMT_SBGGR8:
case V4L2_PIX_FMT_SBGGR12:
width = pix->width;
break;

@@Then, We get the image below:

pastedImage_14.png

However, if we modify "mx6s_capture.c"
{
.name = "RAWRGB12 (SBGGR12)",
.fourcc = V4L2_PIX_FMT_SBGGR12,
.pixelformat = V4L2_PIX_FMT_SBGGR12,
.mbus_code = MEDIA_BUS_FMT_SBGGR12_1X12,
.bpp = 1,
},

@@We get the image below:

pastedImage_17.png

(C).The case which we capture video image with with heavily noise:

#modify "fsl-imx8mm-evk.dts"
&csi1_bridge {
fsl,mipi-mode;
fsl,two-8bit-sensor-mode;
status = "okay";
.......................................
};

#modify "mx6s_capture.c"
case V4L2_PIX_FMT_SBGGR12://RAW12
cr18 |= BIT_MIPI_DATA_FORMAT_RAW12;
break;

@@We get the image below:

pastedImage_34.png

(D). RAW12 Capturer and Player

We use "yavta" to capture raw12 video from our board
#yavta -c100 -p -fSBGGR12 -s 1280x960 -F/home/root/output.raw /dev/video0

And, uisng ffplay to play raw12 video in PC.
#ffplay.exe -video_size 1280x960 -pixel_format bayer_bggr16be output.raw

(E). Our Question:

(1). As we know, i.MX8M is different from i,MX7D, but i.MX8M-Mini is the same as imx7D. So, we want to know whether the configuration between i.MX8M and i.MX8M-Mini is the same ? When we set configuration as (C) (fsl,two-8bit-sensor-mode + BIT_MIPI_DATA_FORMAT_RAW12), the result seems more negative with heavily noise.

(2). How to solve "multiple sensor images"(分屏) in (B) ? It may be happened in i.MX8M Mini, not in i.MX8M.

(3). Do you have suggestion which tool can capture raw12 video ? And, which tool can play raw12 video in PC ?

Thanks a lot for your help.

Sincerely,

TC.Chou

标签 (1)
标记 (3)
0 项奖励
3 回复数

1,884 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello TC,

Below is feedback from i.mx expert team:

------------------

For 1, the MIPI CSI2 modules are different between iMX8MM and iMX8MQ, but the CSI bridges are same.

 

For 2, you need check the frame width setting and camera resolution, another thing should be checked is the preview software.

 

For 3, nxp has the application  note AN12060 "Software ISP Application Note" which can be used to handle the RAW images on board, you can find it from nxp.com.

-------------------

Hope above answers can help you.

Have a ncie day!

B.R,

Weidong

0 项奖励

1,884 次查看
tcchoub
Contributor I

Hello Weidong,

 

For 2, 

In mipi-csi frame size, we modify "mxc_mipi_csi.c":
val = mf->width | (mf->height << 16);
mipi_csis_write(state, MIPI_CSIS_ISPRESOL_CH0, val);

After I print "mf->width" and "mf->height", it's 1280x960.

 

In Camera, we output 1280x960 resolution.

Therefore,  they are the same.

 

Besides, because gstreamer can't support RAW12 video, we use yavta on .i.MX8MM board and ffplay(ffmpeg) it on PC.

#yavta -c100 -p -fSBGGR12 -s 1280x960 -F/home/root/output.raw /dev/video0

#ffplay.exe -video_size 1280x960 -pixel_format bayer_bggr16be output.raw

 

For 3, 

AN12060 "Software ISP" seems not support i.MX8MM

 

Our Question:

(A). Does "MIPI Serial clock Frequency" mean MIPI data rate for "each lane" or "total lane" (See the following table) ?

(B).  1280x960x30(fps)x12(bit) = 442,368,000 = 450Mbps. But, MIPI-CSI is dual-edge. So, we need 225(450/2) MHz. Is it correct ?

 

MIPI Serial clock Frequency (MHz)

HSSETTLE[7:0]

CLKSETTLECTL[1:0]

,1500

33

0

1490~1450

32

0

1440~1410

31

0

1400~1360

30

0

1350~1320

29

0

1310~1270

28

0

1260~1230

27

0

1220~1180

26

0

1170~1130

25

0

1120~1090

24

0

1080~1040

23

0

1030~1000

22

0

990~950

21

0

940~910

20

0

900~860

19

0

850~820

18

0

810~770

17

0

760~730

16

0

720~680

15

0

670~640

14

0

630~590

13

0

580~550

12

0

540~500

11

0

490~460

10

0

450~410

9

0

400~370

8

0

360~320

7

0

310~280

6

0

270~230

5

0

220~190

4

0

180~140

3

0

130~100

2

0

90~80

1

0

 

Thanks a lot for your help.

 

Sincerely,

TC.Chou 

0 项奖励

1,884 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello TC,

See below,  please!
--------------------

For Q(A), each lane. it is the MIPI clock lane frequency * 2.

For Q(B), it is wrong, the calculation should include blank timing, so it should be: pixel clock frequency * bpp / lanes.

--------------------

Hope i.MX Expert's answers can help you!

Have a nice day!

B.R,

Weidong

0 项奖励