i.MX8M Mini - USB isochronous transfer fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Mini - USB isochronous transfer fail

183件の閲覧回数
Jamie01
Contributor I

Hi,

We cannot get the following USB camera to work and start streaming.

libuvc calls "libusb_submit_transfer fail return -1". This is USB isochronous transfer failing. It failed when uvc_stream_start USB was transferring.

It seems the issue could be related to i.MX8M Mini USB full speed. We tested the same camera sample on the other board with i.MX8M Plus CPU. It works out normally. 

Please help to solve this issue. 

 

Please find the following link for the camera specs: 

PureThermal 2

https://groupgets-files.s3.amazonaws.com/PT2/PureThermal%202%20-%20Datasheet%20-%201.7.pdf

Lepton_Series

https://groupgets-files.s3.amazonaws.com/lepton/Resources/Lepton%20Series%20Datasheet.pdf

 

0 件の賞賛
返信
2 返答(返信)

140件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

Which board are you using?

0 件の賞賛
返信

179件の閲覧回数
Jamie01
Contributor I
By the way, it shows "[ 940.873815] usb 1-1: usbfs: usb_submit_urb returned -28"
From kernel's USB driver error log
0 件の賞賛
返信