i.MX8 h.264 encoder bit rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 h.264 encoder bit rate

Jump to solution
1,485 Views
ko-hey
Senior Contributor II

Hi all,
 
I have a question about H.264 encoder in i.MX8.
 
According to the reference manual(Table 15-8) of i.MX8MMini, the bit rate is as below.
Minimum: 10kbps
Maximum: 40 Mbps at 1080p 60 fps
 
How about is it in i.MX8 ?
 
Ko-hey

0 Kudos
Reply
1 Solution
1,383 Views
joanxie
NXP TechSupport
NXP TechSupport

i.MX8 QM B0 supports two HW encoders each one associated to a Cortex-M0. Each HW encoder is capable of encoding 1x H.264 1080p30 or 2x H.264 720p30.

View solution in original post

0 Kudos
Reply
3 Replies
1,383 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the imx8qm data sheet, for encoder, imx8QM supports up to 1080p@30,should be the 20M bps, no data for min

0 Kudos
Reply
1,383 Views
ko-hey
Senior Contributor II

Hi joanxie

It's worse than i.MX8MMini. Are you sure ?

Ko-hey

0 Kudos
Reply
1,384 Views
joanxie
NXP TechSupport
NXP TechSupport

i.MX8 QM B0 supports two HW encoders each one associated to a Cortex-M0. Each HW encoder is capable of encoding 1x H.264 1080p30 or 2x H.264 720p30.

0 Kudos
Reply