Hi,
I have a question regarding the i.MX7 USB_OTG1_VBUS terminal. Could you please assist?
The reason for these questions is that I could not find voltage information in the spec sheet beyond the absolute maximum rating of 5.25V. Also, from the EVA circuit diagram, I understood it to be kept low when the i.MX7 is not powered on. I would like to confirm whether it's okay to directly connect from the USB terminal or use a resistor divider.
Solved! Go to Solution.
Hi Ritesh M Patel,
Thank you for your response. After scrutinizing the information provided, I understand that the circuit diagram based on the EVA is rational. I will create a circuit diagram following the EVA.
Thanks,
HOTA
Hi Ritesh M Patel,
Thank you for your response. After scrutinizing the information provided, I understand that the circuit diagram based on the EVA is rational. I will create a circuit diagram following the EVA.
Thanks,
HOTA
Hi @HOTA,
I hope you are doing well.
Please see the response to your questions below:
[NXP]: It follows the USB 2.0 standard. It is 5.0V +/- 5% i.e. 4.75V.
[NXP]: It is as per the USB 2.0 Standard (5.0V +/- 5%) i.e. 4.75V.
[NXP]: It is not recommended to apply voltage on VBUS when the i.MX is not powered.
[NXP]: The voltage level of VDD_USB_OTG1_3P3_IN and USB_OTG1_VBUS are different. So, they cannot be directly connected.
[NXP]: Yes.
Thanks & Regards,
Ritesh M Patel