i.MX7's USB_OTG1_VBUS threshold and some questions.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7's USB_OTG1_VBUS threshold and some questions.

Jump to solution
629 Views
HOTA
Contributor III

Hi,
I have a question regarding the i.MX7 USB_OTG1_VBUS terminal. Could you please assist?

 

  1. What is the threshold voltage for i.MX7's USB_OTG1_VBUS?
  2. What is the design default voltage for OTGTUNE0 (VBUS Valid Threshold Adjustment) set at 100b?
  3. Is it okay to apply voltage to VBUS when the i.MX is not powered on?
  4. If always in device mode (including serial download mode), can VDD_USB_OTG1_3P3_IN and USB_OTG1_VBUS be directly connected and used?
  5. Us USB_OTG2_VBUS the same in terms of these characteristics?

The reason for these questions is that I could not find voltage information in the spec sheet beyond the absolute maximum rating of 5.25V. Also, from the EVA circuit diagram, I understood it to be kept low when the i.MX7 is not powered on. I would like to confirm whether it's okay to directly connect from the USB terminal or use a resistor divider.

0 Kudos
Reply
1 Solution
607 Views
HOTA
Contributor III

Hi Ritesh M Patel,

Thank you for your response. After scrutinizing the information provided, I understand that the circuit diagram based on the EVA is rational. I will create a circuit diagram following the EVA.

Thanks,

HOTA

View solution in original post

0 Kudos
Reply
2 Replies
608 Views
HOTA
Contributor III

Hi Ritesh M Patel,

Thank you for your response. After scrutinizing the information provided, I understand that the circuit diagram based on the EVA is rational. I will create a circuit diagram following the EVA.

Thanks,

HOTA

0 Kudos
Reply
614 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @HOTA,

I hope you are doing well.

Please see the response to your questions below:

  • What is the threshold voltage for i.MX7's USB_OTG1_VBUS?

[NXP]: It follows the USB 2.0 standard. It is 5.0V +/- 5% i.e. 4.75V.

  • What is the design default voltage for OTGTUNE0 (VBUS Valid Threshold Adjustment) set at 100b?

[NXP]: It is as per the USB 2.0 Standard (5.0V +/- 5%) i.e. 4.75V.

  • Is it okay to apply voltage to VBUS when the i.MX is not powered on?

[NXP]: It is not recommended to apply voltage on VBUS when the i.MX is not powered.

  • If always in device mode (including serial download mode), can VDD_USB_OTG1_3P3_IN and USB_OTG1_VBUS be directly connected and used?

[NXP]: The voltage level of VDD_USB_OTG1_3P3_IN and USB_OTG1_VBUS are different. So, they cannot be directly connected.

  • Us USB_OTG2_VBUS the same in terms of these characteristics?

[NXP]: Yes.

Thanks & Regards,
Ritesh M Patel