Hi All,
Please help in resolving the issue of suspending the CPUs'.
When I poweron the boot process goes smooth and after boot it is suspending the CPUs
Throws the following prints.
Freezing user space processes ... (elapsed 0.02 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.
add wake up source irq 51
PM: suspend of devices complete after 120.017 msecs
PM: late suspend of devices complete after 0.652 msecs
Disabling non-boot CPUs ...
CPU1: shutdown
CPU2: shutdown
CPU3: shutdown
The attached is the full log from logcat. I'm using a custom hardware where I don't have any buttons to configure for wakeup.
I'm stuck here. Please help me to resolve.
Thanks to all.
Original Attachment has been moved to: imx6q_android_4.2.2_logcat.txt.zip
Trilokesh
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
Hi,
Can you share your kernel cmdline?
Regards,
Yamil
Hi Yamail garcia,
the below is my command line arguments.
Kernel command line: console=ttymxc3,115200 calibration enable_wait_mode=off no_console_suspend androidboot.hardware=freescale androidboot.console=ttymxc3 init=/init vmal
loc=256M video=mxcfb0:Primeview-PM070WL4,bpp=32 fbmem=10M,28M video=mxcfb1:hdmi,1280x1024M@60,bpp=32 if=RGB24 vt.global_cursor_default=0 consoleblank=0 board_mx6q_phyflex.csi0=none board_mx6q_phyflex.csi1=none ip=none root=/dev/mmcblk0p2 rootfstype=ext4 noinitrd rootwait mtdparts=n25q128:512k(barebox)ro,128k(bareboxenv),2M(splash),-(kernel);gpmi-nand:512k(barebox)ro,128k(bareboxenv),2M(splash),8M(kernel),-(root)
Trilokesh
We have not got your response yet and will close the diacussion in 3 days.
Thanks,
Yixing
Did you ever get your suspend issue resolved, or is it still an issue for you?