Hi,
We have designed our board using i.MX6UL processor with reference of i.MX6UL EVK only difference is Botting media SD card is on SD1 channel while in EVK booting channel is SD2.
the booting msg of baords as given below
U-Boot 2015.04imx_v2015.04_4.1.15_1.2.0_ga+gede7538 (Apr 22 2017 - 15:12:20)
CPU: Freescale i.MX6UL rev1.2 at 396 MHz
CPU: Temperature 31 C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 512 MiB
force_idle_bus: sda=0 scl=0 sda.gp=0x1d scl.gp=0x1c
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Using default environment
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc0 is current device
Net: FEC0
Error: FEC0 address not set.
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
switch to partitions #0, OK
mmc0 is current device
** No partition table - mmc 0 **
** No partition table - mmc 0 **
Booting from net ...
*** ERROR: `ethaddr' not set
*** ERROR: `ethaddr' not set
My boards not booting ahead from above msg.
While same SD card booted up to linux login in i.MX6UL EVK.
Regards,
Pramod Kumar
Hi Pramod
for sd1 programming one can use mfg tool with script mfgtool2-yocto-mx-evk-sdcard-sd1.vbs
and use correct "mmcblkN" parameter as described in attached document Table 10. Common kernel boot parameters
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------