i.MX6UL DDR data lines

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL DDR data lines

517 Views
surendrajadhav
Contributor IV

Hello,

Let me know for DDR3L interface of .MX6UL, does CPU supports the pin swapping features for data lines.With this feature we can connect any of the data line (D0:16) to any of the data lines. No one to one connection is required i.e. D0 to D0, D1 to D1 and so on.

This helps us for PCB layout.

Regards,

Surendra

Labels (1)
0 Kudos
Reply
1 Reply

407 Views
igorpadykov
NXP Employee
NXP Employee

Hi Surendra

please refer to sect.3.5.1 Swapping data lines

Hardware Development Guide for the i.MX 6UltraLite Applications Processor

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6ULHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply