Can i.MX6SoloX support 12MPx camera sensor and it's full resolution throughput without any slowdown all the way to the memory?
Hi,
For the 12MPx camera sensor, the data output by camera is RAW data, in the i.MX6SX there is no ISP moudule, so it can not work on the i.MX6SX.
In the i.MX6 design, need your camera with the ISP function. The mux clock of CSI is 264MHz, your camera resolution work clock should below the mux value. So, the1080P @30 can work.
Have a nice day
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------