i.MX6SoloX support 12MPx camera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SoloX support 12MPx camera

504件の閲覧回数
stefankolody
Contributor I

Can  i.MX6SoloX support 12MPx camera sensor and it's full resolution throughput without any slowdown all the way to the memory?

ラベル(1)
0 件の賞賛
返信
1 返信

434件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

For the 12MPx camera sensor, the data output by camera is RAW data, in the i.MX6SX there is no ISP moudule, so it can not work on the i.MX6SX.

In the i.MX6 design, need your camera with the ISP function. The mux clock of CSI is 264MHz, your camera resolution work clock should below the mux value. So, the1080P @30 can work.

Have a nice day

Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信