Hi all
Let me confirm about input voltage from PF3000 to VDD_ARM_IN of i.MX6SL.
The device is as below.
・CPU:MCIMX6L2EVN10AB
・PMIC:MC32PF3000A4EP
According to the table 9 of IMX6SLCEC, the min voltage of VDD_ARM_IN for operation at 996MHz is 1.375V.
https://www.nxp.com/docs/en/data-sheet/IMX6SLCEC.pdf
On the other hand, the voltage setting for SW1A of MC32PF3000A4EP is 1.375V.
https://www.nxp.com/docs/en/data-sheet/PF3000.pdf
Q1.
According to the above value, I think I need to set more higher value for SW1A after boot up.
Because there are no margin between them.
Do you recommend to set more higher value for SW1A ?
Q2.
If Q1 is yes, please tell me the recommendation value.
Ko-hey
Hi Ko-hey
1. yes
2. one can use next setting, 1.400V.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------