i.MX6SDL SD Boot Fusemap looks strange

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SDL SD Boot Fusemap looks strange

736件の閲覧回数
torus1000
Contributor V

Hi,

Regard to SD/eSD Boot Fusemap description of i.MX6SDL/DQ reference manual,
It looks different and in-compatible.

i.MX 6Solo/6DualLite
   0 - Internal loopback
   1 - External pad

i.MX 6Dual/6Quad
   0 - through SD pad
   1 - direct

Was it typo? or Should I change this bit if I choose "pad"?

Can anyone help me?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

653件の閲覧回数
art
NXP Employee
NXP Employee

There is some confusing wording in the i.MX6S/DL Reference Manual document. The description of the i.MX6D/Q Reference Manual is correct and more clear. The BOOT_CFG1[0] fuse bit should remain 0 (intact) to take the loopback clock from a pad.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信