Hi everone,
My new desinged i.MX6Q board stopped during linux boot up. U-boot version is 2009.08 and bootargs setting as below:
......
nfsroot=/srv/rootfs
bootargs_base=setenv bootargs console=ttymxc0,115200
bootargs_nfs=setenv bootargs $ root=/dev/nfs ip=dhcp nfsroot=$:$,v3,tcp bootcmd_net=run bootargs_base bootargs_nfs; tftp uImage; bootm bootargs_mmc=setenv bootargs $ ip=dhcp root=/dev/mmcblk0p1 rootwait
bootcmd_mmc=run bootargs_base bootargs_mmc; mmc dev 0; mmc read $ 0x80
0 0x2000; bootm
bootcmd=run bootcmd_net
......
I boot the NFS filesystem but it stopped at--Freeing init memory: 208K ---,the boot log is as below:
Load address: 0x10800000
Loading: * #################################################################
done
Bytes transferred = 3951152 (3c4a30 hex)
Booting kernel from Legacy Image at 10800000 ...
Image Name: Linux-3.0.35-2666-gbdde708
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3951088 Bytes = 3.8 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 3.0.35-2666-gbdde708 (root@lab-linux) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #94 SMP PREEMPT Fri Aug 8 15:00:55 CST 2014
CPU: ARMv7 Processor revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Ignoring unrecognised tag 0x54410008
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @8c80e000 s5440 r8192 d15040 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 454656
Kernel command line: console=ttymxc0,115200 root=/dev/nfs ip=dhcp nfsroot=192.168.2.130:/srv/rootfs,v3,tcp
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
Memory: 512MB 1280MB = 1792MB total
Memory: 1805212k/1805212k available, 291940k reserved, 360448K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xf4600000 - 0xffe00000 ( 184 MB)
vmalloc : 0xea800000 - 0xf2000000 ( 120 MB)
lowmem : 0x80000000 - 0xea000000 (1696 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.init : 0x80008000 - 0x8003c000 ( 208 kB)
.text : 0x8003c000 - 0x80ab5540 (10726 kB)
.data : 0x80ab6000 - 0x80b198a0 ( 399 kB)
.bss : 0x80b198c4 - 0x80b65a98 ( 305 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
arm_max_freq=800MHz
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole enabled
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
CPU2: Booted secondary processor
CPU3: Booted secondary processor
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 at 0
mxs-dma mxs-dma-apbh: initialized
print_constraints: SPKVDD: 4200 mV
print_constraints: vmmc: 3300 mV
vgaarb: loaded
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
mc_pfuze 1-0008: recv failed!:-5,80
mc_pfuze: probe of 1-0008 failed with error -1
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
cfg80211: Calling CRDA to update world regulatory domain
max17135 2-0048: PMIC MAX17135 for eInk display
i2c-core: driver using legacy suspend method
i2c-core: driver using legacy resume method
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 65536 (order: 6, 262144 bytes)
TCP established hash table entries: 262144 (order: 9, 2097152 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 262144 bind 65536)
TCP reno registered
UDP hash table entries: 1024 (order: 3, 32768 bytes)
UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PMU: registered new PMU device of type 0
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = ea880000 suspend_iram_base=ea8f0000
PM driver module loaded
iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.
PCIE: imx_pcie_pltfm_probe start link up.
IMX PCIe port: link up.
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
PCI: bus2: Fast back to back transfers disabled
pci 0000:03:00.0: disabling ASPM on pre-1.1 PCIe device. You can enable it with 'pcie_aspm=force'
PCI: bus3: Fast back to back transfers disabled
PCI: bus4: Fast back to back transfers enabled
PCI: bus5: Fast back to back transfers enabled
PCI: bus6: Fast back to back transfers enabled
PCI: bus7: Fast back to back transfers enabled
PCI: bus8: Fast back to back transfers enabled
pci 0000:00:00.0: BAR 0: assigned
pci 0000:00:00.0: BAR 0: set to (PCI address )
pci 0000:00:00.0: BAR 8: assigned
pci 0000:00:00.0: BAR 6: assigned
pci 0000:01:00.0: BAR 0: assigned
pci 0000:01:00.0: BAR 0: set to (PCI address )
pci 0000:03:00.0: PCI bridge to
pci 0000:03:00.0: bridge window
pci 0000:03:00.0: bridge window
pci 0000:03:00.0: bridge window
pci 0000:02:01.0: PCI bridge to
pci 0000:02:01.0: bridge window
pci 0000:02:01.0: bridge window
pci 0000:02:01.0: bridge window
pci 0000:02:04.0: PCI bridge to
pci 0000:02:04.0: bridge window
pci 0000:02:04.0: bridge window
pci 0000:02:04.0: bridge window
pci 0000:02:05.0: PCI bridge to
pci 0000:02:05.0: bridge window
pci 0000:02:05.0: bridge window
pci 0000:02:05.0: bridge window
pci 0000:02:07.0: PCI bridge to
pci 0000:02:07.0: bridge window
pci 0000:02:07.0: bridge window
pci 0000:02:07.0: bridge window
pci 0000:02:09.0: PCI bridge to
pci 0000:02:09.0: bridge window
pci 0000:02:09.0: bridge window
pci 0000:02:09.0: bridge window
pci 0000:01:00.0: PCI bridge to
pci 0000:01:00.0: bridge window
pci 0000:01:00.0: bridge window
pci 0000:01:00.0: bridge window
pci 0000:00:00.0: PCI bridge to
pci 0000:00:00.0: bridge window
pci 0000:00:00.0: bridge window
pci 0000:00:00.0: bridge window
PCI: enabling device 0000:01:00.0 (0140 -> 0143)
PCI: enabling device 0000:02:01.0 (0140 -> 0143)
PCI: enabling device 0000:03:00.0 (0140 -> 0143)
PCI: enabling device 0000:02:04.0 (0140 -> 0143)
PCI: enabling device 0000:02:05.0 (0140 -> 0143)
PCI: enabling device 0000:02:07.0 (0140 -> 0143)
PCI: enabling device 0000:02:09.0 (0140 -> 0143)
IMX usb wakeup probe
add wake up source irq 75
IMX usb wakeup probe
cpu regulator mode:ldo_enable
i.MXC CPU frequency driver
highmem bounce pool size: 64 pages
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 2821
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
regulatorget: get() with no identifier
imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb
mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd
mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb
mxc_sdc_fb mxc_sdc_fb.3: ipu1-di0 already in use
mxc_sdc_fb: probe of mxc_sdc_fb.3 failed with error -16
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console enabled, bootconsole disabled
console enabled, bootconsole disabled
loop: module loaded
No sata disk.
m25p80 spi0.0: unrecognized JEDEC id ffffff
GPMI NAND driver registered. (IMX)
FEC Ethernet Driver
fec_enet_mii_bus: probed
iwl4965: Intel(R) Wireless WiFi 4965 driver for Linux, in-tree:
iwl4965: Copyright(c) 2003-2011 Intel Corporation
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1
egalax_ts 1-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
elan - Read Hello Packet Failed
elan-touch: probe of 2-0010 failed with error -5
i2c-core: driver using legacy suspend method
i2c-core: driver using legacy resume method
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
i2c-core: driver using legacy suspend method
i2c-core: driver using legacy resume method
usb 2-1: new full speed USB device number 2 using fsl-ehci
mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!
mma8451: probe of 0-001c failed with error -22
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
Galcore version 4.6.9.6622
Thermal calibration data is 0x5544d069
Thermal sensor with ratio = 175
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
Cirrus Logic CS42888 ALSA SoC Codec Driver
i2c-core: driver using legacy suspend method
i2c-core: driver using legacy resume method
imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.
wm8962 0-001a: Failed to get supply 'DCVDD': -19
wm8962 0-001a: Failed to request supplies: -19
wm8962 0-001a: asoc: failed to probe CODEC wm8962.0-001a: -19
asoc: failed to instantiate card wm8962-audio: -19
imx_3stack asoc driver
Initialize HDMI-audio failed. Load HDMI-video first!
ALSA device list:
No soundcards found.
NET: Registered protocol family 26
TCP cubic registered
NET: Registered protocol family 17
lib80211: common routines for IEEE802.11 drivers
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: vmmc: incomplete constraints, leaving on
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
eth0: Freescale FEC PHY driver (mii_bus:phy_addr=1:00, irq=-1)
usb 2-1: device descriptor read/64, error -71
usb 2-1: device descriptor read/64, error -71
usb 2-1: new full speed USB device number 3 using fsl-ehci
usb 2-1: device descriptor read/64, error -71
usb 2-1: device descriptor read/64, error -71
usb 2-1: new full speed USB device number 4 using fsl-ehci
usb 2-1: device not accepting address 4, error -71
usb 2-1: new full speed USB device number 5 using fsl-ehci
usb 2-1: device not accepting address 5, error -71
hub 2-0:1.0: unable to enumerate USB device on port 1
PHY: 1:00 - Link is Up - 100/Full
Sending DHCP requests .
., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.2.118
IP-Config: Complete:
device=eth0, addr=192.168.2.118, mask=255.255.255.0, gw=192.168.2.10,
host=192.168.2.118, domain=, nis-domain=(none),
bootserver=0.0.0.0, rootserver=192.168.2.130, rootpath=, mtu=576
VFS: Mounted root (nfs filesystem) on device 0:12.
Freeing init memory: 208K
Has anyone met this problem? Or some advice to debug it?
Thanks in advance!
Best Regards
Xiaoqiang
解決済! 解決策の投稿を見る。
I would suggest to remove USB hub completely from build and try.
"ip=none" "ip=dhcp" - do not remove USB hub from build.
Hi Xiaoqiang
you can try demo images below and not use dhcp
(use "ip=none" as kernel boot parameter)
L3.0.35_4.1.0_DEMO_IMAGE_BSP :
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you! I followed your method but new situation appeared. The kernel can not go to that place but stops at USB section.
........
........
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: Freescale On-Chip EHCI Host Controller
usb usb1: Manufacturer: Linux 3.0.35-2666-gbdde708 ehci_hcd
usb usb1: SerialNumber: fsl-ehci.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: Freescale On-Chip EHCI Host Controller
usb usb2: Manufacturer: Linux 3.0.35-2666-gbdde708 ehci_hcd
usb usb2: SerialNumber: fsl-ehci.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1
egalax_ts 1-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
elan - Read Hello Packet Failed
elan-touch: probe of 2-0010 failed with error -5
i2c-core: driver using legacy suspend method
i2c-core: driver using legacy resume method
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
i2c-core: driver using legacy suspend method
i2c-core: driver using legacy resume method
usb 2-1: new full speed USB device number 2 using fsl-ehci
mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!
mma8451: probe of 0-001c failed with error -22
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
Galcore version 4.6.9.6622
Thermal calibration data is 0x5544d069
Thermal sensor with ratio = 175
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
Cirrus Logic CS42888 ALSA SoC Codec Driver
i2c-core: driver using legacy suspend method
i2c-core: driver using legacy resume method
imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.
wm8962 0-001a: Failed to get supply 'DCVDD': -19
wm8962 0-001a: Failed to request supplies: -19
wm8962 0-001a: asoc: failed to probe CODEC wm8962.0-001a: -19
asoc: failed to instantiate card wm8962-audio: -19
imx_3stack asoc driver
Initialize HDMI-audio failed. Load HDMI-video first!
ALSA device list:
No soundcards found.
NET: Registered protocol family 26
TCP cubic registered
NET: Registered protocol family 17
lib80211: common routines for IEEE802.11 drivers
VFP support v0.3:
implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: vmmc: incomplete constraints, leaving on
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:06:49 UTC (409)
usb 2-1: device descriptor read/64, error -71
usb 2-1: device descriptor read/64, error -71
usb 2-1: new full speed USB device number 3 using fsl-ehci
usb 2-1: device descriptor read/64, error -71
usb 2-1: device descriptor read/64, error -71
usb 2-1: new full speed USB device number 4 using fsl-ehci
usb 2-1: device not accepting address 4, error -71
usb 2-1: new full speed USB device number 5 using fsl-ehci
usb 2-1: device not accepting address 5, error -71
hub 2-0:1.0: unable to enumerate USB device on port 1
INFO: task ipu1_task:373 blocked for more than 120 seconds.
"echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.
ipu1_task D 804a137c 0 373 2 0x00000000
[<804a137c>] (__schedule0x258/0x6d4) from [<8033c878>] (ipu_task_thread0x260/0
xaf0)
[<8033c878>] (ipu_task_thread0x260/0xaf0) from [<80092740>] (kthread0x80/0x88)
[<80092740>] (kthread0x80/0x88) from [<80041a5c>] (kernel_thread_exit0x0/0x8)
Kernel panic - not syncing: hung_task: blocked tasks
[<80047dc8>] (unwind_backtrace0x0/0xf8) from [<8049d868>] (panic0x64/0x17c)
[<8049d868>] (panic0x64/0x17c) from [<800ad758>] (watchdog0x224/0x24c)
[<800ad758>] (watchdog0x224/0x24c) from [<80092740>] (kthread0x80/0x88)
[<80092740>] (kthread0x80/0x88) from [<80041a5c>] (kernel_thread_exit0x0/0x8)
CPU0: stopping
[<80047dc8>] (unwind_backtrace0x0/0xf8) from [<8003b30c>] (do_IPI0x14c/0x174)
[<8003b30c>] (do_IPI0x14c/0x174) from [<800409cc>] (__irq_svc0x4c/0xe8)
Exception stack(0x80a13f68 to 0x80a13fb0)
3f60: 00000001 80000093 80a13f98 f40c4000 80a12000 80a71564
3f80: 80a27a70 804a5aa4 80a2ad2c 412fc09a 00000000 00000000 00000000 80a13fb0
3fa0: 804a3568 80041abc 40000013 ffffffff
[<800409cc>] (__irq_svc0x4c/0xe8) from [<80041abc>] (default_idle0x24/0x28)
[<80041abc>] (default_idle0x24/0x28) from [<80041cd0>] (cpu_idle0xd8/0x11c)
[<80041cd0>] (cpu_idle0xd8/0x11c) from [<800088a0>] (start_kernel0x238/0x278)
[<800088a0>] (start_kernel+0x238/0x278) from [<10008040>] (0x10008040)
CPU2: stopping
[<80047dc8>] (unwind_backtrace0x0/0xf8) from [<8003b30c>] (do_IPI0x14c/0x174)
[<8003b30c>] (do_IPI0x14c/0x174) from [<800409cc>] (__irq_svc0x4c/0xe8)
Exception stack(0xe9fb5f90 to 0xe9fb5fd8)
5f80: 00000001 80000093 e9fb5fc0 f40c4000
5fa0: e9fb4000 80a71564 80a27a70 804a5aa4 80a2ad2c 412fc09a 00000000 00000000
5fc0: 00000000 e9fb5fd8 804a3568 80041abc 40000013 ffffffff
[<800409cc>] (__irq_svc0x4c/0xe8) from [<80041abc>] (default_idle0x24/0x28)
[<80041abc>] (default_idle0x24/0x28) from [<80041cd0>] (cpu_idle0xd8/0x11c)
[<80041cd0>] (cpu_idle+0xd8/0x11c) from [<10499d94>] (0x10499d94)
CPU3: stopping
[<80047dc8>] (unwind_backtrace0x0/0xf8) from [<8003b30c>] (do_IPI0x14c/0x174)
[<8003b30c>] (do_IPI0x14c/0x174) from [<800409cc>] (__irq_svc0x4c/0xe8)
Exception stack(0xe9f01f90 to 0xe9f01fd8)
1f80: 00000001 80000093 e9f01fc0 f40c4000
1fa0: e9f00000 80a71564 80a27a70 804a5aa4 80a2ad2c 412fc09a 00000000 00000000
1fc0: 00000000 e9f01fd8 804a3568 80041abc 40000013 ffffffff
[<800409cc>] (__irq_svc0x4c/0xe8) from [<80041abc>] (default_idle0x24/0x28)
[<80041abc>] (default_idle0x24/0x28) from [<80041cd0>] (cpu_idle0xd8/0x11c)
[<80041cd0>] (cpu_idle+0xd8/0x11c) from [<10499d94>] (0x10499d94)
Our usb hub is USB2514.And usb is supported in kernel configuration.
From: Igor Padykov
Date: 2014-08-11 09:49
To: Xiaoqiang Yang
Subject: Re: - i.MX6Q stopped during linux boot up
i.MX6Q stopped during linux boot up
reply from Igor Padykov in i.MX Community - View the full discussion
Hi Xiaoqiang
you can try demo images below and not use dhcp
(use "ip=none" as kernel boot parameter)
L3.0.35_4.1.0_DEMO_IMAGE_BSP http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif :
Best regards
chip
do you mean that
without hub (remove USB2514 driver) board is running OK ?
Best regards
chip
no, with usb hub the board can run, but if use"ip=none" it can't run.
xiaoqiang.yang@realtimes.cn
From: Igor Padykov
Date: 2014-08-11 21:34
To: Xiaoqiang Yang
Subject: Re: - i.MX6Q stopped during linux boot up
i.MX6Q stopped during linux boot up
reply from Igor Padykov in i.MX Community - View the full discussion
do you mean that
without hub (remove USB2514 driver) board is running OK ?
Best regards
chip
Reply to this message by replying to this email, or go to the message on Freescale Community
Start a new discussion in i.MX Community by email or at Freescale Community
Following i.MX6Q stopped during linux boot up in these streams: Inbox
NO,
if I use "ip=none" as kernel boot parameter, the kernel stopped after this sentence "hub 2-0:1.0: unable to enumerate USB device on port 1";
if I use "ip=dhcp" as kernel boot parameter,the kernel passed dhcp section and stopped after "Freeing init memory: 208K",
our usb2514 is designed onboard and it seems that usb is not the real phenomenon. I think the real reason must be hiding behind them.
How do you see it?
Best Regards
Xiaoqiang
From: Igor Padykov
Date: 2014-08-11 21:34
To: Xiaoqiang Yang
Subject: Re: - i.MX6Q stopped during linux boot up
i.MX6Q stopped during linux boot up
reply from Igor Padykov in i.MX Community - View the full discussion
do you mean that
without hub (remove USB2514 driver) board is running OK ?
Best regards
chip
Reply to this message by replying to this email, or go to the message on Freescale Community
Start a new discussion in i.MX Community by email or at Freescale Community
Following i.MX6Q stopped during linux boot up in these streams: Inbox
I would suggest to remove USB hub completely from build and try.
"ip=none" "ip=dhcp" - do not remove USB hub from build.
I use "ip=dhcp" and modified my DDR3 configuration(not modified before) and finally boot up the linux. Thank you!
Hello
We are having the same situation here but I don´t find where the DDR3 configuration is made within linux. I only configured the u-boot ddr3 file.
Thank you
We are the same,we only configured DDR3 in u-boot.It seems like linux needn't to configure the DDR.
Hello.
It seems so. Just a while ago, I do what I had to do two days ago: run a network capture program on a third computer and see what is happening. My board is mounting the nfs root and doing some initial directory checking (i suppose) but when the file transfers start many of the board packets are not answered by the nfs server. So the load is really slow. I think the linux is starting but very slowly.
I am installing the root nfs in another computer to see if it goes better.
If anybody knows how to activate some debug-messages on the init process of linux to know what the init process is trying to do, I will thank that anybody. I looked for it but I was unable to found.
Thank you,
Jose
Hello
Here there were two things.
1) One line on the Ethernet connector was bad. After we correct it, speed was good but still nothing was being seen in console.
2) CONFIG_DEVTMPFS was disabled in linux configuration. We activated it, rebuilt and it started to print things in console.
Thank you,
Jose