Hi,
I have 1920x1080 LVDS panel and modified device tree source (dtsi) of i.mx6q yocto L.3.10.53.
Then I tried ldb split mode (ldb=spl0) as following.
U-Boot> setenv displayinfo video=mxcfb1:dev=ldb,if=RGB24 ldb=spl0 fbmem=24M
...
U-Boot> boot
...
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw
video=mxcfb1:dev=ldb,if=RGB24 ldb=spl0 fbmem=24M
...
LVDS1 looked OK but LVDS0 (neither clock nor data) output nothing.
Can anyone help me to output both LVDS ports in split mode(2 ports for 1 panel)?
Actual fbset was as following...
> fbset
mode "960x1080-52"
# D: 74.250 MHz, H: 60.861 kHz, V: 52.018 Hz
geometry 960 1080 960 1088 16
timings 13468 60 60 23 22 140 45
rgba 5/11,6/5,5/0,0/0
endmode
Thanks.
解決済! 解決策の投稿を見る。
Dear Saurabh and Guanqiong,
Freescale local FAE kindly sent us a patch as following.
After applying this patch, it worked.
It seems additional "split-mode;" line required to resolve my issue.
Hava a nice day!
//patch//
--- a/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
+++ b/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
@@ -505,46 +505,47 @@
&ldb {
status = "okay";
+ split-mode;
lvds-channel@0 {
fsl,data-mapping = "spwg";
...
did you add your lvds to the ldb.c? pls refer to the link as below:
Dear Saurabh and Guanqiong,
Freescale local FAE kindly sent us a patch as following.
After applying this patch, it worked.
It seems additional "split-mode;" line required to resolve my issue.
Hava a nice day!
//patch//
--- a/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
+++ b/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
@@ -505,46 +505,47 @@
&ldb {
status = "okay";
+ split-mode;
lvds-channel@0 {
fsl,data-mapping = "spwg";
...
Hello,
How do I do to apply this changes to a new .sdcard?
Thanks.
Hi Torus
Thanks for posting the solution.
Saurabh
Hi
Torus
You need to add display information to struct fb_videomode ldb_modedb according to your resolution.
Can you try to verify ldb driver and dtb file initialization?
Why you have selected video=mxcfb1 ? You can use video=mxcfb0 with dtb setting.
Thanks
Saurabh