i.MX6Dual RTC_XTALI,RTC_XTALO pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Dual RTC_XTALI,RTC_XTALO pins

Jump to solution
931 Views
佐藤智幸
Contributor I

Dear community,

I have a question about i.MX6Dual.

When I do not use external RTCXTAL(32.768k), is the RTC_XTALI,RTCXTALO pin good as a float?

Thanks and Best Regards,

Labels (1)
0 Kudos
1 Solution
686 Views
igorpadykov
NXP Employee
NXP Employee

Hi 佐藤智幸

you should always use RTCXTAL(32.768k) due to

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
687 Views
igorpadykov
NXP Employee
NXP Employee

Hi 佐藤智幸

you should always use RTCXTAL(32.768k) due to

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos