i.MX6DQ ERR005768 and boot device.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DQ ERR005768 and boot device.

ソリューションへジャンプ
553件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ ERR005768.

I want to know the relationship between boot device and ERR005768.

I believe ERR005768 can occur when use NAND as boot device since secondary image is prepared generally when NAND is used.

How about other boot device?

ERR005768 can occur with other boot device? (e.g. eMMC, Parallel NOR, etc...)

Best Regards,

Satoshi Shimoda

ラベル(2)
タグ(1)
0 件の賞賛
1 解決策
451件の閲覧回数
art
NXP Employee
NXP Employee

The ERR005768 silicon erratum is applicable to all boot modes that support redundant boot. These modes are:

-NAND Flash boot;

-SD/MMC/eMMC boot;

-SATA boot.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
452件の閲覧回数
art
NXP Employee
NXP Employee

The ERR005768 silicon erratum is applicable to all boot modes that support redundant boot. These modes are:

-NAND Flash boot;

-SD/MMC/eMMC boot;

-SATA boot.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛