i.MX6DL hangs at when disabling CACHE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DL hangs at when disabling CACHE

ソリューションへジャンプ
916件の閲覧回数
SLICE
Contributor IV

Dear team,

My customer is facing the issue that i.MX6DualLite can hang when executing an instruction which disables CACHE after resuming from suspend mode.

This issue can occur on the customer’s board.

They found the hang-up occurs at when the following instruction was executed.

 

1573         /*

1574          * Restore control register but don't enable Data caches here.

1575          * Caches will be enabled after restoring MMU table entry.

1576          */

1577         ldmea         r0!, {r4}

1578         mov r11, r4

1579         ldr         r2, =CACHE_DISABLE_MASK

1580         and         r4, r4, r2

1581         mcr         p15, 0, r4, c1, c0, 0

1582         isb

 

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/mach-mx6/mx6_suspend.S?h=i...

The above is the source code of Android which is executed when resuming from suspended mode. And it seems to handle CACHE mode.

When i.MX6DL execute the instruction of line-1581, i.MX6DL hangs.

Could you show me why i.MX6DL can hang when manipulating CACHE mode?

And could you please show me the workaround?

 

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
795件の閲覧回数
art
NXP Employee
NXP Employee

Dear Miyamoto,

As far as I understand, the issue is the same as discussed in the original case #00105430 in Salesforce. So, I continue working on the case there, so, further, please refer to this original case #00105430.

Also, I noticed that the customer uses very early 13.4.1 Android BSP. Ask them to try the latest Marshmallow 6.0.1_2.1.0 BSP, whose source code, pre-built images and corresponding documentation are available on the i.MX6/i.MX7 Software Center web page:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

on their affected boards. It should improve the situation. If not, I will escalate the issue to R&D with all the details, found so far.

Best Regards,
Artur

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
796件の閲覧回数
art
NXP Employee
NXP Employee

Dear Miyamoto,

As far as I understand, the issue is the same as discussed in the original case #00105430 in Salesforce. So, I continue working on the case there, so, further, please refer to this original case #00105430.

Also, I noticed that the customer uses very early 13.4.1 Android BSP. Ask them to try the latest Marshmallow 6.0.1_2.1.0 BSP, whose source code, pre-built images and corresponding documentation are available on the i.MX6/i.MX7 Software Center web page:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

on their affected boards. It should improve the situation. If not, I will escalate the issue to R&D with all the details, found so far.

Best Regards,
Artur

0 件の賞賛
返信
795件の閲覧回数
SLICE
Contributor IV

Hello Artur,

Thanks.

Yes, this is same as case #00105430.

Best Regards,

Miyamoto

0 件の賞賛
返信