Hello,
In iMX6QD RM it says
"Fully compliant with MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.2/4.3/4.4/4.41" and
also it says in boot section :
Boot code supports following standards.
• MMCv4.4 or less
• eMMCv4.4 or less
• SDv2.0 or less
• eSDv2.10 rev-0.9, with or without FAST_BOOT.
• SDXCv3.0
Two different statements above made me confused. The question is can i use eMMCv4.41 for fast boot mode of i.mx6?
Thanks in advance..
解決済! 解決策の投稿を見る。
Yes, the boot ROM supports eMMC version 4.41 for fast boot.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
(ref. SR #1-987173450)
The i.MX6 supports fast boot, as it is stated in section 67.4.9 (MMC fast boot)
of the i.MX6 DQ Reference Manual.
Best regards
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, it is apparent that it supports MMC fast boot but the question is whether e.MMC version 4.41 is supported for fast boot.
Yes, the boot ROM supports eMMC version 4.41 for fast boot.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
(ref. SR #1-987173450)
Ok thank you very much, i guess freescale should update the reference manuel and datasheet with the supoorted eMMC versions.