i.MX6 and PCIe GBE controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 and PCIe GBE controller

跳至解决方案
936 次查看
JHY
Contributor IV

Hi, I need second ethernet interface for i.MX6 and plan to use PCIe GBE controllers.

Is there reference test results of PCIe GBE controller about compatibility or real perfomance?

标签 (1)
标记 (4)
0 项奖励
1 解答
583 次查看
igorpadykov
NXP Employee
NXP Employee

Hi conan

I am afraid such performance figures are not available.

One can look at PCIe performance at link below

i.MX6Q PCIe EP/RC Validation System

Any PCIe specs compliant device should work with i.MX6 PCIe module.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
584 次查看
igorpadykov
NXP Employee
NXP Employee

Hi conan

I am afraid such performance figures are not available.

One can look at PCIe performance at link below

i.MX6Q PCIe EP/RC Validation System

Any PCIe specs compliant device should work with i.MX6 PCIe module.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励