i.MX6 and PCIe GBE controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 and PCIe GBE controller

Jump to solution
1,101 Views
JHY
Contributor IV

Hi, I need second ethernet interface for i.MX6 and plan to use PCIe GBE controllers.

Is there reference test results of PCIe GBE controller about compatibility or real perfomance?

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
748 Views
igorpadykov
NXP Employee
NXP Employee

Hi conan

I am afraid such performance figures are not available.

One can look at PCIe performance at link below

i.MX6Q PCIe EP/RC Validation System

Any PCIe specs compliant device should work with i.MX6 PCIe module.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
749 Views
igorpadykov
NXP Employee
NXP Employee

Hi conan

I am afraid such performance figures are not available.

One can look at PCIe performance at link below

i.MX6Q PCIe EP/RC Validation System

Any PCIe specs compliant device should work with i.MX6 PCIe module.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply