i.MX6 and PCIe GBE controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 and PCIe GBE controller

ソリューションへジャンプ
937件の閲覧回数
JHY
Contributor IV

Hi, I need second ethernet interface for i.MX6 and plan to use PCIe GBE controllers.

Is there reference test results of PCIe GBE controller about compatibility or real perfomance?

ラベル(1)
タグ(4)
0 件の賞賛
1 解決策
584件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi conan

I am afraid such performance figures are not available.

One can look at PCIe performance at link below

i.MX6Q PCIe EP/RC Validation System

Any PCIe specs compliant device should work with i.MX6 PCIe module.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
585件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi conan

I am afraid such performance figures are not available.

One can look at PCIe performance at link below

i.MX6Q PCIe EP/RC Validation System

Any PCIe specs compliant device should work with i.MX6 PCIe module.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛