Hi,
I am porting a Linux 3.18.19 kernel on a board which features an i.MX6.
I would like to use it as a real USB OTG, ie as a device or as a host depending on the USB_OTG_ID pin: when low the interface act as a host, when high it acts as a device.
The hardware is OK, as the USB OTG is working as host or device with a Linux 3.0.35 kernel.
When I connect a USB stick to USB OTG, it is enumerated.
When I connect USB OTG to a host PC and "modprobe g_mass_storage", the USB OTG is enumerated by the host PC.
I also see on the a scope that the USB_OTG_ID pin is correctly driven.
With the 3.18.19 kernel, I cannot have both device and host working as expected, even if the USB_OTG_ID is correctly driven.
I can only have one feature working, depending on dr_mode value in the the device tree.
1) &usbotg {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usbotg>;
vbus-supply = <®_5p0v>;
disable-over-current;
dr_mode = "otg";
status = "okay";
};
=> USB OTG can enumerate a USB stick (host OK), but cannot be enumerated by a host PC (device NOK)
After connecting to a host PC, I see the following output in dmesg: ci_hdrc ci_hdrc.0: timeout waiting for 00000800 in 11
2)
&usbotg {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usbotg>;
vbus-supply = <®_5p0v>;
disable-over-current;
dr_mode = "peripheral";
status = "okay";
};
=> USB OTG is enumerated by the host PC (device OK), but it cannot enumerate a USB stick (host NOK)
This seems normal, as the USB OTG is described as a peripheral, so it cannot work as a host.
What am I missing to have USB OTG working as a real OTG in case 1) ?
Regards,
David
3.18 is not a supported kernel version. Please use a recent kernel (4.1 from NXP or 4.13.2 from mainline) and let us know if you face these issues.
Hi David,
As suggested by Linux device tree, dr_mode="otg" has to support the real OTG mode.
Actually for the first case,ci_hdrc is the host USB driver. It says Timeout.
Can you please share the debug log here for investigation?
Also, it will be great if you can share the behaviour for the following changes:
Host functionality by setting dr_mode="host".
Thanks,
Ramya
Please Use freescale standard BSP release
L3.10.17, L3.10.53, L3.14.28 to try.