Does mainline kernel support SDIO of i.MX25

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does mainline kernel support SDIO of i.MX25

1,045件の閲覧回数
Sun1z
Contributor III

I use mainline kernel 3.10.102, now I tested two sdio devices but both of them can be recognized but can't work properly, on the same port, SD card works fine. I wonder is there any patch need to applied to mainline kernel?

B.R.

Nus

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

882件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Please try 4.13.2 instead.

There have been some recent patches that improve SD/MMC operation on MX25. Please see the latest 4 patches

Benoît Thébaudeau:

https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux-stable.git/log/drivers/mmc/host/sdhci-e... 

0 件の賞賛
返信

882件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

In our website no such patch. Here you can refer to https://community.nxp.com/docs/DOC-1468 .

0 件の賞賛
返信