i.MX6 SoloX: does GPT_CLK support a 1GHz clock ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 SoloX: does GPT_CLK support a 1GHz clock ?

675 次查看
xav
Contributor II

Hi,

everything's in the title: is it possible to input a precise external 1GHz clock into the GPT to timestamp signals to the nanosecond ?

Thanks,

        Xav

0 项奖励
回复
1 回复

613 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

unfortunately this is not possible, only arm core can work

with 1GHz frequency, other peripherals not.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复