i.MX6 SoloX: does GPT_CLK support a 1GHz clock ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SoloX: does GPT_CLK support a 1GHz clock ?

639 Views
xav
Contributor II

Hi,

everything's in the title: is it possible to input a precise external 1GHz clock into the GPT to timestamp signals to the nanosecond ?

Thanks,

        Xav

0 Kudos
Reply
1 Reply

577 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

unfortunately this is not possible, only arm core can work

with 1GHz frequency, other peripherals not.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply