i.MX6 Dual in 32-bit DDR3 configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Dual in 32-bit DDR3 configuration

ソリューションへジャンプ
836件の閲覧回数
rafaeldelrey
Contributor I

Hello,

I need to redesign an i.MX6 Dual design, pursuing to lower costs with only 2 DDR3 ICs instead of 4 in the original design.

Due to cost reasons (my main target), this is cheaper than jumping to LP-DDR2 memories.

Also due to SW reasons, as far as I know, I need to stick to i.MX6 Dual device.

The question is: Can I leave DQ[32-64] and their respective DQS signals disconnected in order to use a true 32-bit memory bus in the i.MX6 Dual? or they (DQ[32-64]) should be terminated somehow (33 to 50 ohms Pullup or pulldown or whatever)?

Thanks

ラベル(1)
1 解決策
582件の閲覧回数
jan_spurek
NXP Employee
NXP Employee
2 返答(返信)
582件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Rafael del Rey,

Please look at the threads suggested by Jan for more details. Unused pins of the DDR controller may be left floating if not used.

Regards,

0 件の賞賛
583件の閲覧回数
jan_spurek
NXP Employee
NXP Employee

Hello Rafael,

please refer to the following threads:

https://community.nxp.com/message/591423

https://community.nxp.com/message/500229

Best Regards,
Jan