i.MX6: Documentation about DVFS related registers in GPC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6: Documentation about DVFS related registers in GPC

1,224 次查看
valterminute_
Contributor I

I noticed that documentation about DVFS in the GPC chapter and specific documentation about DVFSC_* registers in that same chapter has been removed in the latest revisions of the reference manual of both i.MX6 dual/quad and solo/duallite.

I am talking about registers from 0x020dC180 to 0x020DC1C0.

The documentation was not very clear, but I was surprised to see it disappear.

I also noticed that those registers are not used in the Linux BSP (where the logic to increase/decrease CPU speed is implemented in software).
On the other side the HW DVFS feature is quite useful for people working on OSs that don't have such a management system built-in. Being able to trigger actions based on system load using HW is quite interesting.

Why has this information been removed?

Is that feature not working or is suggested to not use it?

Has this information been moved to a different place?

(no mention about this in the revision notes that just say that it has been deleted)

标签 (4)
0 项奖励
回复
3 回复数

917 次查看
igorpadykov
NXP Employee
NXP Employee

Hi valterminute

hardware dvfs module was used in older i.MX processors, like i.MX53,

in i.MX6 it is not used and related information was removed from documentation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

917 次查看
valterminute_
Contributor I

What does "not used" mean?

As far as I could see the registers are there.

They should not be used because there are some hardware issues?

0 项奖励
回复

917 次查看
igorpadykov
NXP Employee
NXP Employee

it was not validated and not used in software bsps.

Best regards
igor

0 项奖励
回复