i.MX6 Audio port (AUDMUX port ) as Input and Output simultaneously

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Audio port (AUDMUX port ) as Input and Output simultaneously

Jump to solution
2,137 Views
ndsonu
Contributor II

Hi All,

We have our audio connection around the i.MX6 as below.

aud_connection.PNG.png

Here, we are trying to use audio port 6 as a transmitter (master)  and receiver (slave)  simultaneously.

AUD6_RX - needs to be a slave and receives I2S audio from INAP375R chip.

AUD6_TX - needs to be an I2S master and will push I2S data to an audio codec ( SGTL5000).

Please note that we have connected two different devices to TX and RX lines of same audio port.

Is this configuration supported/allowed  from both HW and SW (Linux) perspective?

Thank you for your support!

Thanks,

Sonu     

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,621 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sonu

yes AUDMUX module supports this hardware configuration.

In software you should write own custom driver for it.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,622 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sonu

yes AUDMUX module supports this hardware configuration.

In software you should write own custom driver for it.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,621 Views
ndsonu
Contributor II

Thank you Chip!!!

0 Kudos
Reply