SABRE Lite, OpenGL ES 2.0, FBO, low performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE Lite, OpenGL ES 2.0, FBO, low performance

2,584 Views
oskarosobniak
Contributor I

Hi

I added FBO support but looks like the performance is much lower than I expected. I'm using two screens (scene rendered for two cameras). Without FBO I have 55 fps. After adding it (texture 1024x768) - it's only 26 fps.

I also checked different configurations:

1. "Slower" - scene rendered 4 times + 2 quads with texture:

- Camera1 to FBO1

- Camera2 to FBO2

- Screen1: Camera1 - fullscreen, Camera2 - FBO2, shown on small quad

- Screen2: Camera2 - fullscreen, Camera1 - FBO1, shown on small quad

Results (for different texture size):

- 256x256 - 50 fps
- 1024x768 - 30 fps
- 2048x2048 - 9 fps

2. "Faster" - scene rendered 2 times + 4 quads with texture:

- Camera1 to FBO1

- Camera2 to FBO2

- Screen1: Camera1 - FBO1, fullscreen, Camera2 - FBO2, shown on small quad

- Screen2: Camera2 - FBO2, fullscreen, Camera1 - FBO1, shown on small quad

Results:

-  256x256 - 43 fps
- 1024x768 - 23 fps
- 2048x2048 - 8 fps

Part of code:

// ## rendering to texture1 ##:

glViewport(0, 0, 1024, 768);

glBindFramebuffer(GL_FRAMEBUFFER, m_FBO);

glClear(GL_COLOR_BUFFER_BIT | GL_DEPTH_BUFFER_BIT);

// drawing scene

glBindFramebuffer(GL_FRAMEBUFFER, 0);

glViewport(0, 0, 1024, 768);

// ## rendering to texture2 ##:

// (performed for 2nd FBO)

eglMakeCurrent(...);// setting screen1

// drawing fullscreen quad with FBO1

// drawing small quad with FBO2

eglSwapBuffers(...);// for screen1

eglMakeCurrent(...);// setting screen2

// drawing fullscreen quad with FBO2

// drawing small quad with FBO1

eglSwapBuffers(...);// for screen2

Do I need to change/add something or the device is not enough fast for using FBO? I'm using SABRE Lite - maybe the problem is related to the device?

Labels (3)
0 Kudos
Reply
1 Reply

798 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oskar

suggest to post this very special issue on

meta-fsl-arm mailing list, so that someone familiar with FBO SABRE Lite

could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

chip

0 Kudos
Reply