Hi community,
I have a questions about i.MX6 ASRC_ASRCTR setting.
Please see chapter 15.7.1 in IMX6SDLRM Rev.1.
I understand pair A will automatic update when ATSA bit is 1, and update manually by USRA and IDRA bit when ATSA bit is 0.
Then, how about when the following setting?
Pair A will automatic update? or ASRC internal measured ratio will be used?
ATSA = 1
USRA = 1
IDRA = 0
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
Pair A will automatic update, based on ASRC internal measured ratio.
Hi Yuri,
According to your reply, ATSA setting and {USRA, IDRA} setting are applied at the same time.
Then, how about {ATSA, USRA, IDRA} = {1,0,0}.
I guess USRA & IDRA is ignored and "Pair A will automatic update its pre-processing and post-processing options based on the frequencies it detected".
Is this correct?
Best Regards,
Satoshi Shimoda
Can somebody reply me?