i.MX6 ARM DS-5 debugger doesn't work with kernels after 3.10.53.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 ARM DS-5 debugger doesn't work with kernels after 3.10.53.

611 次查看
norishinozaki
Contributor V

Hello,

ARM DS-5 debugger works fine with kernel 3.10.17 on i.MX6DL/QSabreSDP

However the version 3.10.53, 3.14.28, 3.14.52 and 4.1.15 doesn't work.

When I connect DS-5 to the running kernel, Sabre hangs.

When I try to boot the kernel with DS-5 connected, it hangs just as explained below.

Is there anyone who knows how to debug(J-TAG) IMX6DL based on 3.14.28 Kernel?

Do I need to change kernel configuration or device tree file?

Should I ask ARM?

BR,

N.S.

标签 (2)
0 项奖励
回复
2 回复数

446 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Have you tried to disable CAAM drivers in kernel?

-> Cryptographic API                                

                               [ ] Hardware crypto devices

Luis

0 项奖励
回复

446 次查看
norishinozaki
Contributor V

Hello Luis,

Thanks, I tried with removing the option right now in 3.14.28.
It worked!!

Thank you & BR,

N.S

0 项奖励
回复