i.MX53 QSB U-Boot tips for testing the board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 QSB U-Boot tips for testing the board.

1,053件の閲覧回数
Claude_Sylvain
Contributor I

- When launching the i.MX53 QSB, press a key on the remote terminal to get
  into U-Boot.
- Then just enter the following command:
    - run bootcmd_obds

- This will load and execute OBDS ("On Board Diagnostic Setup"), and allow
  you to test your i.MX53 QSB board.


- Remark: This apply to the Freescale BSP.


Claude



ラベル(1)
0 件の賞賛
返信
2 返答(返信)

779件の閲覧回数
Claude_Sylvain
Contributor I


>
> Is the OBDS contained in uboot somewhere?
>

- Probably, but I never done in depth search on "OBDS"; so
  I am not absolutely sure.


>
> I downloaded the OBDS source code, and need some guidance on the
> switches for the makefile.  (I'm trying to use the QSB w/the
> non-freescale PMIC).  Can you help w/this?
>

Sorry, but I can not help you on that point.


Claude



0 件の賞賛
返信

779件の閲覧回数
BenBeckwith
Contributor I

Is the OBDS contained in uboot somewhere?  I downloaded the OBDS source code, and need some guidance on the switches for the makefile.  (I'm trying to use the QSB w/the non-freescale PMIC).  Can you help w/this?

Thanks,

Ben

0 件の賞賛
返信