I am trying to run DDR stress test using USB on i.MX53 custom
board. (DDR3 RAM of size 256MB, running at 400MHz)
It runs calibration and asks for details such as frequency.
Then asks for ddr frequency (125 to 400 in steps of 5MHz).
Then the test runs smoothly upto 550MHz. But after that i'm not
seeing any progress, and also no error/success information.
Please suggest solution.
Thanks.
With regards,
Keshava G N
解決済! 解決策の投稿を見る。
IMX63 ESDCTL supports memory frequency up to 400 MHz.
550 MHz is out of specified range.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
IMX63 ESDCTL supports memory frequency up to 400 MHz.
550 MHz is out of specified range.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri Muhin.
could you support me DDR3 stress test Script. the CPU is IMX536. DDR is MT41K256M16 – 32 Meg x 16 x 8 banks.
could you help me modify the Parameters and i want to set up at my delphi board
thanks, Yang Liu
Hello,
Please try to create SR - it helps me to not forget this issue.
Have a great day,
Yuri
Thanks for answer, Yuri !!
Can you please look into my another similar question :
??
Thanks again... :smileyhappy: