i.MX53 DDR3 stress test hangs at DDR clock 550

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 DDR3 stress test hangs at DDR clock 550

Jump to solution
1,336 Views
KeshavaGN
Contributor V

I am trying to run DDR stress test using USB on i.MX53 custom

board. (DDR3 RAM of size 256MB, running at 400MHz)

It runs calibration and asks for details such as frequency.

Then asks for ddr frequency (125 to 400 in steps of 5MHz).

Then the test runs smoothly upto 550MHz. But after that i'm not

seeing any progress, and also no error/success information.

Please suggest solution.

Thanks.

With regards,

Keshava G N

Labels (1)
0 Kudos
Reply
1 Solution
884 Views
Yuri
NXP Employee
NXP Employee

IMX63 ESDCTL  supports memory frequency up to 400 MHz.

550 MHz is out of specified range.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
885 Views
Yuri
NXP Employee
NXP Employee

IMX63 ESDCTL  supports memory frequency up to 400 MHz.

550 MHz is out of specified range.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
884 Views
yanglius
Contributor I

Dear Yuri Muhin.

could you support me DDR3 stress test Script. the CPU is IMX536. DDR is MT41K256M16 – 32 Meg x 16 x 8 banks.

could you help me modify the Parameters and i want to set up at my delphi board

thanks, Yang Liu

0 Kudos
Reply
884 Views
Yuri
NXP Employee
NXP Employee

Hello,

Please try to create SR - it helps me to not forget this issue.


Have a great day,
Yuri

0 Kudos
Reply
884 Views
KeshavaGN
Contributor V

Thanks for answer, Yuri !!

Can you please look into my another similar question :

i.MX53 DDR3 stress test - Not working for correct configuration

??

Thanks again... :smileyhappy: