i.MX35 Clock Tree Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX35 Clock Tree Tool

1,352件の閲覧回数
JesseBeeker
Contributor III
Here is a new tool to understand and configure the clocking system on the i.MX35x product. GUI complete with installation and user guide. We are working on getting it on the Freescale website but we will get out to the community as we wait.

Original Attachment has been moved to: 856-i.MX35ClockTreeTool.zip

タグ(1)
0 件の賞賛
6 返答(返信)

1,099件の閲覧回数
JesseBeeker
Contributor III
It has come to my attention that Windows 7 seems to be left out of the picture as well. People can weigh in as needed but I would expect most users to be XP based. Thanks Jon for identifying this. Jesse Beeker said:
Works with Windows. Sorry to offend the tribe.
0 件の賞賛

1,099件の閲覧回数
JonNibert
Contributor I
Additionally, if you used an installed to run the Alpha version, you will likely need to remove the older install using Control Panel >> Add/Remove Program. If the installer for future versions could provide a way to automatically remove the old one, I think that could make updating easier.
0 件の賞賛

1,099件の閲覧回数
JesseBeeker
Contributor III
Please try the newly posted .zip version. Unzip and run the exe. You must have .net 3.5 installed but it will tell you if you don't have it.
0 件の賞賛

1,099件の閲覧回数
JesseBeeker
Contributor III
I see this problem myself. Not good. I will re-upload.
0 件の賞賛

1,099件の閲覧回数
TerryHomeOffice
Contributor I
The i.MX35ClockTreeTool.rar file cannot be downloaded. Indicates that I do not have permissions to access the file. Terry
0 件の賞賛

1,099件の閲覧回数
JesseBeeker
Contributor III
Works with Windows. Sorry to offend the tribe.
0 件の賞賛